AnsweredAssumed Answered

Building dhcp result in an error during patching

Question asked by matt67 on May 2, 2016
Latest reply on May 3, 2016 by Carlos_Musich

Dear all,

I use the BSP imx-4.1.15-1.0.0_ga with en imx6ul evk board and I try to add the dhcp server in the image. I do not modify (nor add bbappend) to the recipe poky/meta/recipes-connectivity/bind/bind_9.10.2-P4.bb

However I'm facing an error from 'quilt'

ERROR: Command Error: exit status: 1  Output:
Usage: quilt [--trace[=verbose]] [--quiltrc=XX] command [-h] ...
       quilt --version
Commands are:


Global options:


--trace
  Runs the command in bash trace mode (-x). For internal debugging.


--quiltrc file
  Use the specified configuration file instead of ~/.quiltrc (or
  /home/matt/DEV/build/tmp/sysroots/x86_64-linux/etc/quilt.quiltrc if ~/.quiltrc does not exist).  See the pdf
  documentation for details about its possible contents.  The
  special value "-" causes quilt not to read any configuration
  file.


--version
  Print the version number and exit immediately.
ERROR: Function failed: patch_do_patch
ERROR: Logfile of failure stored in: xxxxx/build/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/bind/9.10.2-P4-r0/temp/log.do_patch.20456
ERROR: Task 648 (/xxxxx/sources/poky/meta/recipes-connectivity/bind/bind_9.10.2-P4.bb, do_patch) failed with exit code '1'

 

I also checked my version of quilt which is 0.60, and I tried 0.63 without success.

The feature is added through CORE_IMAGE_EXTRA_INSTALL += "dhcp-server dhcp-client" in conf/local.conf

Any tweaks ?

Outcomes