We've been developing an application on a FRDM-KL43Z board but now want to port it to our custom board with a KL17. I notice that the driver set for the two is nearly identical with the exception of a line in the clocks about USB. Is it necessary to convert the project, and if so how do we properly do this?
Hello Kenneth,
Do you said the kl17256?
If yes, yes ,you can download the project about frdm-kl43 into kl17.
While i recommend you create one project on KDS about KL17, then copy
the application code on kl43 board in to the project , then download it .
Hope it helps
Alice