Hello joseph
56F84789 has two ADC modules: 16bit SAR ADC and 12bit Cyclic ADC.
The attached example is a project for SAR ADC which is working in hardware triggering mode.
In addition, user can download the example projects for 56F84789 from:
The example package is under ‘Software Development Tools -> Lab and Test Software’ in the above page.
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks for the sample project , it will a great help if u could suggest a document(specific application note or something) to under stand the adc functionality in mc56f84789 properly
Hello joseph
For details of ADC functionality, please refer to the reference manual:
http://cache.nxp.com/files/dsp/doc/ref_manual/MC56F847XXRM.pdf
For the ADC conjunction with other modules, you may refer to:
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4583.pdf
Hope this helps!
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------