I've seen something about the USBDM but could not find the compatibility from a 2X series to a 1X series.
As well I am using KDS and not the code warrior.
best regards
Hello Niko,
Do you meaning download the code about MKL15Z128CAD4R in to the board FRMK-KL25,
yes ,it can .
And when you debug, please configure the debug view to KL25z128 chip .
Hope it helps
Alice
Oh, I think you got me at the wrong and of the stick.
As far as I know you can use the FRDM MKL25Z Board as a debugger for external devices.
On our own board we are using the MKL15Z128CAD4R.
Therefore I want to know if it is possible to use the external debug function from the FRDM Board to debug our MKL15ZCAD4R?
Best regards
Niko
Von: Alice_Yang
Gesendet: Freitag, 29. April 2016 10:35
An: Nikolaos Theodoridis
Betreff: Re: - Hey Guys, is it possible to use the MKL25Z FRDM Board to program the MKL15Z128CAD4R?
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Hey Guys, is it possible to use the MKL25Z FRDM Board to program the MKL15Z128CAD4R?
reply from Alice_Yang<https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion<https://community.freescale.com/message/640279?et=watches.email.thread#comment-640279>
Hello Niko,
Sorry to reply to so late, have your problem be resolved ?
If not ,there is a tutorial about use the FRDM-KL43 board to debug external board,
https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/
it is the same debug chip on FRDM-KL25 and FRDM-KL43, so the method is the same,
hope it can help you .
BR
Alice