Where can I find MKW01 Radio Utility_.exe to download?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find MKW01 Radio Utility_.exe to download?

1,143 Views
gj35
Contributor II

No one at Freescale seems to know where or how to access the MKW01 Radio Utility_JA.exe that is required for the MRB-KW01 Demo unit.   I have not been able to located it anywhere.

8 Replies

911 Views
antonioconcio
NXP Employee
NXP Employee

Hello,

You can download the Radio Utility Application from the tab "Software & Tools" of the KW01 web page, under the section Board Support Packages.

Let me past here below the link directly:

KW0x|Kinetis KW0x Sub-1 GHz Radio MCUs|NXP

Cheers,

Antonio

911 Views
gj35
Contributor II

Thanks for the info.

Any idea why all the menus options are “grayed” out when I run this program? It allows no changes to be made.

Thanks,

Grant Juel

0 Kudos

911 Views
antonioconcio
NXP Employee
NXP Employee

Hi Grant,

You have to plug the MRB-KW01 board into PC first before to run the application.

Also please be sure you have the USB2SER Drivers installed.

Cheers,
Antonio

0 Kudos

911 Views
gj35
Contributor II

The drivers were loaded.

The board was connected prior to activating the program.

…………..all “grayed” out…………..

0 Kudos

911 Views
antonioconcio
NXP Employee
NXP Employee

Hi Grant,

Did you click on the connection icon?

pastedImage_0.png

I don't face any issue with that, running on Windows 7 machine.

Cheers,

Antonio

0 Kudos

911 Views
gj35
Contributor II

It says “connection could not be established.”

0 Kudos

911 Views
antonioconcio
NXP Employee
NXP Employee

Could you please check if the COM port has been recognized from Windows? Unplugging and re-plugging the cable?

Cheers,

Antonio

0 Kudos

911 Views
gj35
Contributor II

When it finally worked it said COM 6 ….

0 Kudos