AnsweredAssumed Answered

Can the NMI be used to generate an interrupt while running?

Question asked by Jason Maranhao on Apr 27, 2016
Latest reply on May 4, 2016 by Fang Li

I want to be able to generate an NMI (Non-Maskable Interrupt) while the processor is running (KL17).  The design is to connect it to an external low power detection IC to trigger when the external power is dropping below a threshold.  We need this interrupt to save some state information to non-volatile memory before the power drops off completely. 

 

Most of the documentation on the Kinetis systems and the KL17 specifically refers to the NMI as being triggered from the system reset.  Is this the only way this interrupt will be triggered or can it be used while the processor is running?

 

Thanks!

Outcomes