Hello Champs,
Regarding ARM Errata 845369:
"ERR009604 ARM (CA9): 845369 — Under very rare timing circumstances, transition into
streaming mode might create a data corruption".
Is not found in the latest SoloX Errata.
Is that because SoloX doesn't have ACP?
Looking at 4.1.15 u-boot code, MX6SOLO doesn't hit this errata also.
include/configs/mx6_common.h
#ifndef CONFIG_MX6UL
#define CONFIG_ARM_ERRATA_743622
#if (defined(CONFIG_MX6QP) || defined(CONFIG_MX6Q) ||\
defined(CONFIG_MX6DL)) && !defined(CONFIG_MX6SOLO)
#define CONFIG_ARM_ERRATA_751472
#define CONFIG_ARM_ERRATA_794072
#define CONFIG_ARM_ERRATA_761320
#define CONFIG_ARM_ERRATA_845369
#endif
BR,
N.S.
Hi Nori
you are right : affected only i.MX6DQ/DL (SoloX doesn't have ACP).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thanks!
N.S.