The belows is from Developing an Application for the i.MX Devices on the Linux Platform ,but i can not search i.MX31 PDK 1.5 Linux User’s Guide ,where can i find it?
If the user requires any help to set up the prerequisites, refer to the Linux BSP documents. For example,for setting up the i.MX31 PDK, refer to the i.MX31 PDK 1.5 Linux User’s Guide (926-77208), which is available in the BSP tarball that resides in the /doc/ directory.
I had found the file below,i think is the file i.MX31 PDK 1.5 Linux User’s Guide
i.MX31 3-Stack Platform Linux SDK
Standard Release Package User’s Guide
Document Number: 926-77208
Rev. 1.2
02/2008
it is located on i.MX31 PDK product page, below full links:
Supporting Information (4)
i.MX35 PDK Linux Documentation Bundle (REV 2009.12)
Board Support Packages (2)
Linux 2.6.31 Source Code Files 2009.12 Release support i.MX23, i.MX25, i.MX35, i.MX51. (REV 2009.12)
~igor