What is the power savings on i.MX 6SoloX when scaling Cortex-A9 frequency to 800MHz, 500MHz, and 300MHz?
How much power can be saved by shutting off the GPU, VPU, and IPU blocks?
Hi Tom
from arm docs : Cortex A9 0.25 mW/Mhz
(250mW @ 1GHz) per http://www.arm.com/products/processors/cortex-a/cortex-a9.php
i.MX6SX has not vpu, seems there are no data for power consumption of separate modules,
one can make comparative analysis using for example data for Use case 1 and case "Typical max power"
from AN5050 i.MX 6SoloX Power Consumption Measurement
http://cache.nxp.com/files/32bit/doc/app_note/AN5050.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------