any one suggest us the Microcontroller which is compiants to IEC61508 standard with lower pin count (less than 100 pins).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

any one suggest us the Microcontroller which is compiants to IEC61508 standard with lower pin count (less than 100 pins).

279 Views
arvapallykumara
Contributor I

Hi,

I am Kumaraswamy from Knorr-Bremse,India.We are working into Railway Braking
domain.

In our Project we are designing SIL2 compliant system. In this we require the
Micro controller compliant to IEC 61508 (ISO26262) safety standard with Lower
Pin count(less than 100).

Kindly suggest the same.

0 Kudos
0 Replies