S12ZVL32 Flash Programmer Fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVL32 Flash Programmer Fail

698 Views
zongliangchan
Contributor I

146075_146075.png1.png

 

circled it is a wrong message!

MCU = S12ZVL32

IDE  = CodeWarrior 10.6

Tool = USB-MultiLink

 

Please Help!

Labels (1)
0 Kudos
4 Replies

488 Views
RadekS
NXP Employee
NXP Employee

Hi Zong,

Could you please share here the whole log from your console?

Flash Programming Console log.png

Files may be attached when you switch editor window into the advanced editor (in right upper corner).

Could you please also specify your operating system (USB BDM Multilink is not supported by PE drivers under Win10)?

It already worked before?

Are there any other error messages?

Could you please create a new empty project for S12ZVL32 and test load it into MCU?

Do you use any device which could externally reset MCU – for example, external watchdog?

If yes, please disconnect external reset from MCU during programming.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

488 Views
zongliangchan
Contributor I

Thank you
In order to solve this problem!

Use 'Flash File To Target' Function, Erase MCU after normal

this is my code cause this problem

0 Kudos

488 Views
RadekS
NXP Employee
NXP Employee

Hi Zong,

Thank you for your post.

Just for clarification: You erased the MCU by Flash programmer tool and now it works? Or this issue was caused by Flash programmer tool?

Best Regards,
RadekS

0 Kudos

488 Views
zongliangchan
Contributor I

Not Flash programmer tool problem

my source code have problem

0 Kudos