Codewarrior for MCU V6.0 can't flash MC9S08PA60, as there isn't service pack for MC9S08PA60 in codewarrior for MCU V6.0. Can V10.6 flash MC9S08PA60?
Thanks a lot!
Hi,
unfortunately MC9S08PA/PT devices can be only supported under CW10.
you can use CW10.6 to edit/buiild/debug/program MC9S08PA60.
if you want to program MC9S08PA60 in standlone mode, please refer this url:
https://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/
can this help you?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Where can I download Service Pack: CW MCU V6.0 for MC9S08AC60 and MC9S08PA60?
Best regard
Hi,
all CW for MCU v6.0 service packs are listed here
CodeWarrior Updates for MCUs v6.0|NXP
from where we can see there is no MC9S08AC60 pack for CW MCU v6.0. CodeWarrior for Microcontrollers v6.0 - AC16 Service Pack can support MC9S08AC16/8 but can't support MC9S08AC60 device.
to work with MC9S08AC60 you can use latest eclipse CW10.6.4 or classic CW6.3. here is the download link
can it help you?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Zhang,
I installed classic CW6.3 in 32bit Windows XP, and try to flash s19 file to MC9S08AC60.
The operation step is: Hi-wave--->File--->Open configuration---->E2006_touch.ini. At this moment, an error occurred. The details is " An error occurred when executing command file: E2006_touch.hwl"
Hello,
this question was answered
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------