I am working with imx6 solo processor with a custom base board which is running android kk 4.4.2.
We have a USB 2.0 HUB connected to SOM on USB_HOST_DP, USB_HOST_DN.
And OTG is connected independent from USB 2.0 HUB to SOM.
When we tried to switch OFF and ON the power to USB 2.0 HUB (which is a GPIO from SOM), peripherals connected to USB HUB is working fine.
When OTG is in slave mode android is not able to work in fastboot / adb.
But it is able to work in HOST mode.
Regards,
M.Muthumani.
Hi Muthumani
for USB OTG one can check if USB connector ID pin is floating
and voltage on porcessor VDD_VBUS_CAP.
Please check also attached document sect.8.2 How do I use Android
fastboot? It makes sense to check OTG in slave mode using MFG Tools:
will it connect and probably with Linux.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------