Codwarrior for MC9S12XET256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codwarrior for MC9S12XET256

638 Views
sandeep_undale
Contributor I

Hi,

 

Which is the right Codwarrior software for MC9S12XET256? Is it only the classic version or a updated version is also available? Is "CodeWarrior for HC12 Professional Edition WIN" right and the only software for it?

 

Regards,

SU

Labels (1)
0 Kudos
2 Replies

322 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello sandeep

MC9S12XET256 is only supported officially in Classic CodeWarrior. The latest version can be downloaded from:

http://tinyurl.com/j4s4fcb

If you would like to use HCS12 on Eclipse CodeWarrior, you may refer to:

Classic - Is it possible (How) to use HCS12 on Eclipse?

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

322 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi SU,

yes, you are correct.

the latest CodeWarrior for HC12  version is v5.2, which can support MC9S12XET256. for more about it, see

CodeWarrior Dev Tools for HCS12(X) MCUs|NXP

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos