AnsweredAssumed Answered

bitbake Error with i.MX6UL-EVK dtb

Question asked by mickaeltoumi on Apr 13, 2016
Latest reply on Apr 13, 2016 by mickaeltoumi

Hello,

 

I ran bitbake last night for the i.MX6UL-EVK platform. The command was: bitbake core-image-base

 

The repository has been synched before the build.

 

I am following the steps in the document called: Freescale_Yocto_Project_User's_Guide.pdf

 

I have the following error:

 

| NOTE: make -j 8 imx6ul-14x14-evk.dtb

| make[3]: *** No rule to make target `arch/arm/boot/dts/imx6ul-14x14-evk.dtb'.  Stop.

| make[2]: *** [imx6ul-14x14-evk.dtb] Error 2

| make[1]: *** [sub-make] Error 2

| make: *** [all] Error 2

| ERROR: oe_runmake failed

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_install (log file is located at /home/mtoumi/yocto_base/fsl-release-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/linux-imx/3.14.28-r0/temp/log.do_install.29429)

ERROR: Task 71 (/home/xxxxx/yocto_base/fsl-release-bsp/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install) failed with exit code '1'

NOTE: Tasks Summary: Attempted 1428 tasks of which 1382 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

 

 

Summary: 1 task failed:

  /home/xxxxx/yocto_base/fsl-release-bsp/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

 

What's missing?

Outcomes