Dear team,
I would like to ask about the SD Card booting used for i.MX6SoloLite.
My customer is using your cfimager-imx tool to make SD-Card for i.MX6SL boot.
From the messages which cfimager displays, they think cfimager writes MBR and its partition tables other than boot-image. Before they use cfimager, they thought the boot image written at the 2nd sector of SD-Card is needed but MBR and partition table is not necessary.
Can I understand that appropriate MBR and partition table are needed for SD-Card as boot device?
Thanks,
Miyamoto
Yes, an SD card should have the valid MBR to use it as a boot media for i.MX6 series processors. For more information, please refer to the Sections 4.3 and 4.6.1 of the attached document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------