AnsweredAssumed Answered

Unable to debug ISF2P2_K22F_MQX_SF_PROJ

Question asked by Mark Sample on Apr 11, 2016
Latest reply on Apr 15, 2016 by Mark Sample

Hello, Using KDS 3.2.0 and SDK 1.2.0. I think I followed all the steps to update KDS and update Processor Expert with ISF2P2_PEx.PEupd. But I am unable to launch the debugger and down load code to the FRDM-K22F board with FRDM-STBC-AGM01. I know the hardware is ok because when I download FSFK-K22F-AGM01-GL-NED.bin and use the Sensor Fusion GUI to flash the board it works great. Here is a screen shot of the error when launching the P&E debugger:

Compiler warnings:

Console output:

I thought the installation might be corrupted so I uninstalled KDS and re-installed. Also un-installed the example program and re-installed.

 

Q1. Any thought on what I'm doing wrong?

 

Q2. The .bin I mentioned above (FSFK-K22F-AGM01-GL-NED.bin). Is the project that generated that file available?

 

Q3. Is there a SF example that uses Bare Metal?

 

Thank you,

Mark

Outcomes