AnsweredAssumed Answered

Trace on Vybrid with DS-5

Question asked by a a on Apr 8, 2016
Latest reply on Apr 18, 2016 by Karina Valencia Aguilar


I am now using TWR-VF65SG10 Tower Board , and I can boot from SD card, by the way I am on windows host

 

I'm trying to use DS-5 to trace on this board, and I follow the step as follow link

 

https://www.google.com.tw/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&uact=8&ved=0ahUKEwjmk7Sfsv_LAhWDGaYKHVZLAQkQF…

 

here's one step

 

"Plug in an Ethernet and connect it to your local PC. The board is set to static IP of 169.254.0.100. Set your PC to something similar like 169.254.0.1."

 

so I unplug my host ethernet cable, and use crossover cable to connect the target board and my host(windows)

 

but the ip address showed from the A5 is 192.168.1.3  so I changed the IP addr to it

 

"Adjust the host’s networking so that it can communicate with the target. TCP/IP (for example Ethernet) is used to communicate with the target when doing application level debug and Streamline profiling"

 

I change my host (win7) IP address to 192.168.1.1 and default gateway to 192.168.1.254

 

but it didn't work

 

I was wondering where did it go wrong,

Outcomes