Hi,
I have tow FlexRay Evaluation Board from ON-semiconductors (NCV73810V2GEVB) which use the MC9S12XF512MLM microcontroller. I've planned to work with Code Warrior V.5.1. for programming it. I will work on FlexRay application. I don't have selected any Suite yet.
I was looking in the attached document which detail the differences between CW Suites and I wondered if the following restriction (or others that I did not see) could be anoying for FlexRay application :
Thanks.
Thank you Alice.
I have now an other question about CW suite. In theProfessional Suite, there is something about OSEK kernel awareness.
Can you tell me more about it ? Is it usefull or even essential for a FlexRay application ? I'm a novice in communication network.
Hello Pierre,
In order to distinguish between different question , please create
another question about your new question , then we will continue
support it at the new thread , thank for your support .
BR
Alice
Hello Pierre,
After you build your project , you can check the real code size on the .map file ,
then select the suite CW license for you .
If still have any question or i misunderstand you , you can tell me without any
hesitate .
BR
Alice