CLRC663 - ISO 18000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 - ISO 18000

1,313 Views
jmunoa
Contributor I

Hello,

I just acquired a 13.56 MHz multiprotocol reader, CLRC663 red board, in order to communicate with SL2S1512FTB tags, that support  ISO/IEC 18000-3 mode 3/EPC Class-1 HF.

The tools available in NXP site include a script based software "RC663 Serial RS 232 Test Program" and some script examples for different protocols such as ISO15693, ISO14443.. but I can't find any script to test this ISO 18000-3.

Does someone know where can I find any scripts for that software that configures the reader in ISO18000 mode?

Thank you very much.

Best regards,

Jon

0 Kudos
1 Reply

915 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jon Munoa:

Thank you for using our NFC  community.

You are right the package unfortunately does not include a script for ICODE tags. There are some examples for ICODE using the CLEV663B blue board together with the NFC Reader Library, under the "Software and Tools" tab in the product page:

High performance NFC reader solution|NXP

Regards!

Jorge Gonzalez

0 Kudos