Dear All,
Device : i.MX6 SoloX (MCIMX6X1CVO08AB)
First, refer to "Table 118. 17x17 mm NP (no PCIe) supplies contact assignments" in IMX6SXIEC(Rev.1).
L9 pin was defined as VDD_SOC_CAP.
Next, refer to attached file.
L9 pin was defined as VDD_SOC_IN* in OrCAD symbol.
Which is right?
Best Regards,
Keita
Solved! Go to Solution.
Hi Keita
it should be VDD_SOC_IN for "L9" pin
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Hello. Thank you for you reply.
> it should be VDD_SOC_IN for "L9" pin
Let me confirm again.
Refer to "Table 127. i.MX 6SoloX Data Sheet Document Revision History" in IMX6SXIEC(Rev.1).
There is below description.
-----
In Table 118, "17x17 mm NP (no PCIe) supplies contact assignments," on page 164, added ball L9 to the VDD_SOC_CAP row
-----
Is the description typo?
If the data sheet's description was typo, could you request about modification the document?
Best Regards,
Keita
Hi Keita
this DS typo will be corrected, as mentioned in application team answer on
https://community.freescale.com/message/628537
you can access to that thread with help of local fae.
Best regards
igor
Dear Igor,
Thank you for your quick response!
OK. Thank you very much.
Best Regards,
Keita
Hi Keita
it should be VDD_SOC_IN for "L9" pin
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------