Does the BSC9132 device tree correct?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the BSC9132 device tree correct?

633 Views
pbeatini
Contributor I

Hello all,

The device tree for the BSC9132 maps the DUART at 0x4500 and 0x4600. It seems to me that these values are correct for BSC9131 but not for the BSC9132 (which should be: 0x4000 and 0x4200) as stated in the BSC9132RM.pdf manual.

Where is the error? in the manual or in the device tree?

Thanks.

Patrick.

Labels (1)
0 Kudos
1 Reply

446 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Patrick Beatini,

DUART memory map for BSC9132 is the same as BSC9131, please refer to the following section in the table "Table 2-2. Power Architecture CCSR Block Base Address Map" in BSC9132RM.pdf, you would understand why DUART registers are defined at 0x4500 and 0x4600 in the device tree.

pastedImage_0.png


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos