AnsweredAssumed Answered

i.MX6 vpu firmware source code

Question asked by Kenji Teranishi on Apr 5, 2016
Latest reply on Apr 5, 2016 by Kenji Teranishi

Hi all,

 

I are developing an encoding application on i.MX6Q Sabre board using Freescale Yocto Project BSP code (imx-3.14.52-1.1.0_ga).

I would like to change rate control (quant param control) of macro-block level.

I think that it is necessary to change the firmware of the VPU. But, there are only a binary file (vpu_fw_imx6q.bin) of the firmware in yocto project.

Can I get the source code of VPU firmware or sample code from somewhere?

 

Best Regards,

Kenji

Outcomes