Dear team,
My customer is developing their board with i.MX6SoloLite, and they are facing the issue about start-up.
What they want to is;
- Using switch connected to ONOFF pin of i.MX6.
- When the first time VDD_SNVS_IN has been fed, PMIC_ON_REQ stays in L.
- When the switch is pushed -> PMIC_ON_REQ outputs H -> PMIC start the power-on sequence.
Against the above, the actual behavior is as below.
When the first time VDD_SNVS_IN had been fed -> PMIC_ON_REQ outputs H -> PMIC starts the power-on sequence.
I think the above behavior is the specification of i.MX6SL, but
Do you have any ideas to realize the customer’s requirement?
Thanks,
Miyamoto
Hello,
Let me look at the scheme. You may send it via case 00073117.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------