AnsweredAssumed Answered

Sabre Board Battery Application

Question asked by Atilla Mete Turedi on Apr 5, 2016
Latest reply on Apr 11, 2016 by Artur Petukhov


Greetings,

 

On Sabre Board for Smart Devices, 2 x MAX8903 modules are proposed for a battery operated version of the board. It is also said that they need to be connected to two Li+ batteries in parallel. Regarding this;

 

1. What type of batteries did NXP test the battery operated version if any thests were done at all? What were the mAh and the size of the batteries planned? How long did the batteries NXP tested, if any conducted, lasted for different operations? Are these information available?

 

2. What type of battery holder was planned to be used with the Sabre board with battery operated version?

 

Best Regards,

Mete

Outcomes