can't download IMX6_L4.1.15_MFG_TOOL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can't download IMX6_L4.1.15_MFG_TOOL

Jump to solution
1,342 Views
浩卢
Contributor III

I can't download IMX6_L4.1.15_MFG_TOOL.But I can download others MTG_TOOL except this.

Labels (1)
0 Kudos
1 Solution
7 Replies
1,007 Views
alanlow
Contributor II

Hi Yuri,

That link is more likely to download L4.1.15_1.0.0_LINUX_DOCS instead of L4.1.15_1.0.0_MFG_TOOL.

0 Kudos
1,007 Views
liu_xiaodong2
Contributor I

Hi Yuri,

   This link is unable to download due to a system outage now. Is there some other place I can get it? 

Thank you~

0 Kudos
1,007 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
1,007 Views
浩卢
Contributor III
0 Kudos
1,007 Views
浩卢
Contributor III

hi Yuri

Thank you.I got it.

0 Kudos