MQX flashx driver READ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX flashx driver READ

776 Views
yoramshacham
Contributor III


flashx driver allows registration of proprietary READ function, however it doesn't seem to use it anywhere.

How can a flash device that requires proprietary read function (for example SPI) be implemented ?

0 Kudos
2 Replies

463 Views
soledad
NXP Employee
NXP Employee

Hello,

You can check the Flashx example code located at the path: C:\Freescale\Freescale_MQX_4_2\mqx\examples

The example demonstrates basic operation we can do with flash memory including writing string of characters into the memory and reading it back. The memory characteristic, reading and writing statuses as well as the data are displayed over output terminal.

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

463 Views
yoramshacham
Contributor III

Hi Sol,

Walking through the examples and driver code it seems that the flashx driver requires SPIFI support within the controller, as the driver read accesses assume that the flash is memory mapped to the MCU.

The READ function registered by the low level driver is not used by the flashx driver.

How can serial flash be used with flashx in devices such as K60, K65, K70 ?

0 Kudos