About keeper pin in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About keeper pin in i.MX6DQ.

Jump to solution
769 Views
keitanagashima
Senior Contributor I

Dear All,

Refer to "Table 100. 21 x 21 mm Functional Contact Assignments" in IMX6DQCEC (Rev.4).

Out of Reset Condition : Keeper

What state is "keeper" out of reset condition (POR_B)?

Best Regards,

Keita

0 Kudos
1 Solution
545 Views
Yuri
NXP Employee
NXP Employee

Hello,

Strictly speaking, initial state of input signals with keep scheme is not defined.

Have a great day,
Yuri
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
546 Views
Yuri
NXP Employee
NXP Employee

Hello,

Strictly speaking, initial state of input signals with keep scheme is not defined.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos