Hello,
Looking at the data sheet and reference manual pinout for the MK06 44 pin LQFP PTB0 is assigned to pin 24 and PTB1 is assigned to pin 23. But ProcessorExpert shows the pins flipped i.e. PTB0 = pin 23 and PTB1 = Pin24. Which is correct?
Thx,
Ronen
Hi All,
That is diagram issue for the position of these two pins on 44LQFP package in data sheet and reference manual.
That is, PTB1 is on pin 23, PTB0 is on pin 24.
The issue is fixed in new version to be published. Thanks.
Hi Ronen,
I am using ProcessorExpert in KDS3.2.0, this version seems correct.
You can try to update the software.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------