Dear team,
My customer wants to use Maxim/MAX9272, Deserializer, for camera input of i.MX6Solo.
As for the parallel output from MAX9272, a spread spectrum(1%) is added.
Can i.MX6SL receive the parallel data from MX9271 correctly?
Thanks,
Miyamoto
Yes, it is possible to use the MAX9272 on the parallel CSI input port of i.MX6SL with 1% spread spectrum on pixel clock/output. Also, please note that the CSI port of i.MX6SL is maximum 16-bit wide, so, the corresponding data format should be selected on the link/deserializer side.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Artur,
Thanks for your answer.
Can i understand that there is no special setting for i.MX6 to receive 1% SS signal?
Thanks,
Miyamoto
No, no special settings are required for i.MX6 to get the 1% spread spectrum CSI input.
Best Regards,
Artur