AnsweredAssumed Answered

I want to Use flexcan interface  of IMX6, currently I am looking a ECU simulator which supprots the ISO 11898 , Based on the infor (Each FlexCAN module is a  communication controller  implementing the CAN  protocol according to Bosch  Specification versio

Question asked by govardhan Mattela on Mar 28, 2016
Latest reply on Jun 8, 2017 by Carlos Oliva

I want to Use flexcan interface  of IMX6, currently I am looking a ECU simulator which supprots the ISO 11898 , Based on the info (Each FlexCAN module is a  communication controller  implementing the CAN  protocol according to Bosch  Specification version 2.0B  and ISO Standard 11898)

Is any  ECU simulator supports the flexcan protocol. How we can prove that the IMX can bus can support other ISO standras. Looking for help

I am able to communicate IMX -IMX with flexcan interface,

Outcomes