Hello,
is there any one experiencing the conflict between LDB interface with MIPI CSI camera interface? I have successfully implemented LVDS and MIPI CSI camera on hummingboard. When I only enable one of them, the system worked perfectly. However, if I enable both of them, MIPI CSI interface will get the following error:
mipi csi can not receive sensor clk
I used uEnv.txt to enable and disable LDB. As long as I configure the display interface to be ldb, even if the lvds is not correctly configured, the MIPI CSI interface will get the clk error.
Hopefully someone can help. Thank you!!
Hi Yuefeng
mipi csi can be used simultaneously with lvds lcd, please refer to the
mxc_vpu_test.out source code and example of usage :
https://community.freescale.com/message/547363#comment-547363
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------