APBH_DMA USED FOR GPMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

APBH_DMA USED FOR GPMI

414 Views
michaelsyh
Contributor I

I read the ”iMX6_Firmware_Guide.pdf“, and I am curious about the DMA command structure uesd in gpmi driver, can I just use the struct "GENERIC_DESCRIPTOR" to operate the DMA channel without using the register such as next command address register.

where can I find the include files used in the test driver, and is there source code related to the code written in the ”iMX6_Firmware_Guide.pdf“?

I am really looking forward to the reply, thanks a lot!

Labels (1)
0 Kudos
1 Reply

287 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please create request in order to get the Platform SDK sources.

How to submit a new question for NXP Support

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos