MX6 Dual Lite SABRE AI CPU Card PMIC Confusion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX6 Dual Lite SABRE AI CPU Card PMIC Confusion

567 Views
ScottKerstein
Contributor III


Hello,

There is some confusion from what the MX6DL SABRE AI CPU Card schematics indicates as the recommended PMIC P/N and what the PMIC datasheet states:

Schematic (sch-27767_a_x3.pdf) and BOM (BOM-27767_A.xlsb) indicates using MMPF0100F0ZES, which has rev'd to MMPF0100F0AZES per the PMIC datasheet.

However, the PMIC datasheet (Rev. 9.0, 12/2015) recommends using the "NP" version of the part if using the MCIMX6DLAICPU1 reference design.  This contradicts the AI schematic which states "F0" should be used.

From the MMPF0100Z datasheet:

mx6dlSABREAICPUe.PNG

From MCIMX6DLAICPU1 schematic:

fromschematic.jpg

What is the recommended PMIC for MCIMX6U6AVM08AC?

Thank you in advance!

Scott

Labels (2)
0 Kudos
1 Reply

350 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Since the non-programmed PMIC uses “NP” as the programming code - it allows

high range adaptation the NP case for customer's designs. But it may be needed

to program PMIC before using.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos