The QorIQ SDK 1.9 manual mentions that the classifier_demo is not available for T1040. I tried to run that demo (with altered Fman RX port/Offline port configuration), but it doesn't work ("fragmentation_demo: Failed to execute the FMC Model"). Is there a hardware restriction for why it shouldn't work?
There is no information for restriction for the classifier_demo on the T1040 board. Look at the following pages:
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
If you look at the first link
It says, and I quote:
Classifier_demo application supports the following platforms:
- P2041
- P4080
- B4860
- B4420
- T4240
- T2080
Nowhere it mentions T1040. The SDK doesn't contain config files for classifier demo for T1040.
This quote together with the fact that it _doesn't_ work suggest that it is not supported. My question is: what's the reason for it not being supported and how can I fix it.
Best regards,
Jakub Horak