DDR3 layout for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 layout for i.MX6

640 Views
ramansubramania
Contributor I

NXP recommendation for the layout of the DDR3 with
a two chip solution is to use a balanced T for the clock, address, and command
lines, which is how it is implemented  on the Saber board.  In
the NXP layout recommendations, you list the lengths of each of the
groups.  In particular, you list the max length of the clock traces to be
no greater than 2.25 inches.  In a balanced T configuration, does this
consider the total length of the T (both branches), or is it the distance from
the iMX6 to a DDR3 pad?

The reason customer is  asking is that they  conform to the latter
but not the former.  Any thoughts/advice/suggestions?

Labels (1)
0 Kudos
1 Reply

340 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raman

max length assumes distance from the iMX6 to a DDR3 pad.

In general if design does not conform this, recommended to perform

ibis modelling for finding optimal layout.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos