I am using imx6dl board ,android 4.4.2, and sometimes when I wake up the lvds , the screen is white
I tried to delay the led_enable to 250ms, but it did not work ,what should I do ? thanks!
Hi feng,
Is the board you designed it yourself? And you porting the LVDS screen to your board? If yes, here the lvds do not work maybe caused by the improper parameter setting, you should according to the screen datasheet. Here you can refer to the thread in our community Porting LVDS LCD With Low Resolution to i.MX6 . The step is almost the same. Hope it can help you.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------