AnsweredAssumed Answered

iMX6UL-EVK: How do I use MFG-TOOL to boot from QSPI Nor Flash?

Question asked by haoliu on Mar 23, 2016
Latest reply on Apr 4, 2017 by Charles Mao
Branched to a new discussion

The iMX6UL-EVK contains 256Mb QSPI Nor Flash. In Serial Download Mode, choose mfgtool2-yocto-mx-evk-spi-nor.vbs to open mfgtool(3.14.52), but found error:

 

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Dec 05 2015 - 02:09:52)

CPU:   Freescale i.MX6UL rev1.0 at 396 MHz

CPU:   Temperature 41 C

Reset cause: POR

Board: MX6UL 14X14 DDR3 ARM2

I2C:   ready

DRAM:  1 GiB

force_idle_bus: sda=0 scl=0 sda.gp=0x3 scl.gp=0x2

Can't find PMIC:PFUZE100

initcall sequence bff92d60 failed at call 87802e90 (err=-1)

### ERROR ### Please RESET the board ###

 

Dose iMX6UL-EVK support to boot from QPI Nor Flash?

Outcomes