Send screen content to Ethernet on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Send screen content to Ethernet on i.MX6

676 Views
liuxiaoming
Contributor I

Hi,

          I have an i.MX6Q SabreSD board on hand and its working fine. Now I want to send the screen content ( including Qt GUI and camera display ) to the Ethernet. Could this concept be realized? Any idea how to start this up?

0 Kudos
2 Replies

427 Views
jorgesoria
Contributor II

If I remember well there were an VNC Server at core-image-sato image. I succesfully connected to it to take screenshots, you can try it to see if framerate meet your needs.

Best regards.

Jorge.

0 Kudos

427 Views
igorpadykov
NXP Employee
NXP Employee

Hi Liu

seems one can start with copying frame buffer data to file,

refer to attached Linux Manual sect.6.4.1 Framebuffer Tests,

then send file through ethernet.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos