To use CLAA-WVGA on i.MX6SoloX SABRE.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To use CLAA-WVGA on i.MX6SoloX SABRE.

1,426 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SX SABRE board.

According to Linux Release Notes (IMXLXRN Rev.L3.14.52_1.1.0-ga), L3.14.52 BSP supports WVGA panel on the i.MX6SX SABRE.

So I tried using CLAA-WVGA (MCIMX51LCD) with the following kernel parameter, but no image was appeared on the screen.

mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot} video=mxcfb0:dev=lcd,CLAA-WVGA,if=RGB656

Any other setting are needed?

Best Regards,

Satoshi Shimoda

Tags (2)
0 Kudos
1 Reply

772 Views
jayaramks
Contributor III
0 Kudos