Linux 3.10.17_1.0.0_ga bootup on IMX6sabrelite board with PCIe adaptor from boundary device. I connect Broadcom WiFi Bluetooth PCIe chipset. I boot the device, PCIe device is detected once, but then PCIe device are never listed again with lspci command. I tried with other PCie device and other IMX6Q board, reset multiple times, lspci never list my device.
Its the first time I work with PCIe, not much knowledge about it.
Do any one face this type of issue. Pls suggest any solution
Hi Paul
one can try attached patch and check below link
PCIe link doesn't come up with XIO2001 PCI bridge on iMX6Q custom board
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------