AnsweredAssumed Answered

Booting issue in imx6 kontron board

Question asked by berlin vince on Mar 22, 2016
Latest reply on Dec 13, 2016 by bateman cai

Hai...

we are using third party board of kontron(smarc -samx6i) using imx6.we are trying to boot using the Yocto document attached here.

U-Boot 2015.04-00025-gaa1cf09 (Jul 21 2015 - 15:28:22)

 

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz
Board: Kontron SMARC-sAMX6
I2C:   ready
DRAM:  1 GiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
SF: Detected W25Q16DW with page size 4 KiB, total 2 MiB
SF: Detected W25Q16DW with page size 4 KiB, total 2 MiB
Display: LCD_1024x768@LVDS (Resolution: 1024x768 [px], LVDS clk 72 [MHz])
In:    serial
Out:   serial
Err:   serial
Selected Boot source: Carrier SD Card
Net:   FEC [PRIME]
Hit any key to stop autoboot:  0
49272 bytes read in 104 ms (461.9 KiB/s)
4565488 bytes read in 264 ms (16.5 MiB/s)
## Booting kernel from Legacy Image at 10800000 ...
   Image Name:   Linux-3.10.17-rel1.0+g232293e
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    4565424 Bytes = 4.4 MiB
   Load Address: 10008000
   Entry Point:  10008000
   Verifying Checksum ... OK
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid

 

could anyone help?

Outcomes