MIPI CSI-2 capabilities vs data lanes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI CSI-2 capabilities vs data lanes

Jump to solution
976 Views
g_moreno
Contributor III

Hello,

About the MIPI CSI-2 capabilities, I would like to confirm if the following calculation is correct: for 1920 x 1080 @ 30 fps in video mode, do I need at least 3 data lanes?

F = 1920 * 1080 * 30 * 1.35 * 2 (cycles per pixel) = 168MHz

According to i.MX6QRM Rev. 2 page 2733, maximum bandwith for 2 lanes is 125MHz.

Thank you!

Labels (2)
0 Kudos
1 Solution
779 Views
igorpadykov
NXP Employee
NXP Employee

Hi Guillermo

I believe your calculations are correct, 3 data lanes are needed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
780 Views
igorpadykov
NXP Employee
NXP Employee

Hi Guillermo

I believe your calculations are correct, 3 data lanes are needed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

779 Views
g_moreno
Contributor III

Thank you Igor.

0 Kudos