AnsweredAssumed Answered

imx6 widescreen on 3.14.52

Question asked by Edward Tyrrell on Mar 21, 2016
Latest reply on Mar 21, 2016 by Edward Tyrrell

Hi,

 

I'm having an issue setting the resolution of a LVDS display to 1280*800 - Wide Screen. The kernel on our custom board is fsl-release-bsp and Jethro version 3.14.52 (duallite).

 

My research shows that this version should use panel=LDB-WXGA and not the boot-args but neither way actually works. Halting uboot shows "unsupported panel LDB-WXGA" question is how and what can I do to get my screen found at the corrent resoultion? The default Hannstar is fine but the last 1/4 is scrambed on this screen.

 

Also does the device tree have to find this display via an i2c probe or can I simply adjust the resoultion to 1280*800 somewhere using the defult Hannstar driver? Can somebody explain this boot procedure for the 3.14.52 kernel?

 

Thanks,

 

Edward

Outcomes