I just download "CodeWarrior for HCS12(X) Microcontrollers v5.2" but it doesn't have hc12xd derivative. I tryied to find it but I didn't.
Hi,
CW5.2 only includes support for the following derivatives. This is NXP market decision:
- MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96
- MC9S12G128, MC9S12G96
- MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64
- MC9S12GN16, MC9S12GN32
- MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128
- MC9S12XEP100, MC9S12XEP768
- MC9S12XEQ384, MC9S12XEQ512
- MC9S12XET256
- MC9S12XS128, MC9S12XS256, MC9S12XS64
- MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64
If you want to use other hcs12(x) devices, We suggest you use CW5.1.
CW for HCS12(x) v5.1 evaluation version can be downloaded from here:
"CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1 "
CW5.1 can also support 32/64bit win7 officially without problem.
however the original install CW5.1 doesn't support some P&E tool such as Multilink FX, in this case if you want to use CW5.1 + Multilink FX, please install Patch for (S)12(X) 3rd Party Software from P&E website:
http://www.pemicro.com/faqs/faq_view.cfm?id=211
can this help you?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------