AnsweredAssumed Answered

1 Gb Ethernet MAC (ENET) system limitation of i.mx 6dual

Question asked by yinghao liu on Mar 21, 2016
Latest reply on Mar 21, 2016 by yinghao liu

Hi,

I want to use i.mx 6dual(soc) in my customized board,but I find a description in “Chip Errata for the i.MX 6Dual/Quad”,that is :"The theoretical maximum performance of 1 Gbps ENET is limited to 470 Mbps (total for Tx and Rx). The actual measured performance in an optimized environment is up to 400 Mbps"

 

I'm just wondering if it would loss package in the transmission when just up to 300 Mbps?

 

Thanks very much,

sasha

Outcomes