IMX53 QSB simple GUI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53 QSB simple GUI

816 Views
didier1
Contributor I

Hi

I need how to build a yocto image like core-image-minimal or core-image-sato but with just a simple GUI, without windows manager on a imx53 board.

Someone could give some indication?

Regards

Seize

Labels (4)
0 Kudos
3 Replies

622 Views
didier1
Contributor I

thx igor

But i have no problem to generate image like core-image-minimal or core-image-sati.

I'd like to use one of this with a minimal graphic use interface, just create and display a picture with graphic and text.

Regars

Seize

0 Kudos

622 Views
igorpadykov
NXP Employee
NXP Employee

H seize

latest official gui bsp is ltib, no yocto releases are provided.

Suggest also post on meta-fsl-arm mailing list

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

0 Kudos

622 Views
igorpadykov
NXP Employee
NXP Employee

H seize

please look at

core-image-minimal Yocto for imx53qsb

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos