Hi all,
According to iMX6Q display adjustment link able to see test application code to change csc matrix values. But actually i didn't see any effect on my imx6q-sabresd lcd touch panel. So my understanding this test application only gives csc matrix values but not reflected to driver side of csc ipu. So my exact question is how to enable csc ipu driver in kernel level to test application for changing brightness, contrast and hue etc.....
And my another doubt......Is imx6q sabresd board support to change brightness, contrast and hue values?
If yes means solution is through csc test application(imx_csc.c). But this is not reflecting into my sabresd board.
Whether I have to do extra setup or Whether I have to enable extra drivers because im very new to csc ipu unit..
Thanks in advance
You can check this code as example about how to change CSC on Display Processor (using the framebuffer driver /dev/fb0). It's possible to change hue, bright, contrast and etc etc...
imx_csc.c work on imx6dlsabresd?, i download it, this is not reflecting into my sabresd board?
Hi chandrasekhar
BSP provides some csc capability using g2d as described in
sect.7.3.15 Video conversion attached Linux Guide.
Regarding ipu, one will have to add such capability using suggestions
in mentioned iMX6Q display adjustment link.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you igor, But while executing kernel command line:
gst-launch-1.0 videotestsrc ! video/x-raw,format=NV12 ! imxvideoconvert_{g2d} ! video/x-
raw,format=RGB16 ! ximagesink display=:0
it shows system/bin/sh: gst-launch-1.0 not found
Will u please help to run gsl-launch-1.0 in freescale imx6 sabresd board??I followed from github GitHub - Freescale/gstreamer-imx: GStreamer 1.0 plugins for i.MX platforms. Is this correct link?? or any reference links from freescale official site..
Hi chandrasekhar
please follow
Board Support Packages (29)
L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)
~igor
I downloaded this package..But actual my board is imx6q sabresd board and I am using linux-3.10.53 as kernel_imx.
After downloading L3.14.52_1.1.0 (L3.14.52_1.1.0 i.MX VivanteVTK file). For what purpose this link will use?
In this tar file if list out
/Downloads/L3.14.52/L3.14.52_1.1.0-ga_gpu-tools$ ls
vAnalyzer.zip vCompiler.zip vTexture.zip
vclCompiler.zip vEmulator.zip vShader.zip vTracer.zip
What i have to do using these zip files....help me