Bill Elliot

CWHC08 v6.1 Functions menu

Discussion created by Bill Elliot on Feb 21, 2008
Latest reply on Feb 25, 2008 by Bill Elliot
I have just recently installed v6.1 (previously using v3.1) and when I click on the "Functions menu" button in the editor the list includes #defines and prototypes in addition to the actual functions that are contained in the source.  Is this the intended behavior now (v3.1 did not do this)?  Is there a way to have the Functions menu only list the functions that are actually defined in the file being edited?
 
Thanks,
 
Bill
 

Outcomes