I have a question about something on the datasheet for P82B715, link provided below.
http://www.nxp.com/documents/data_sheet/P82B715.pdf
On page 7 it says:
"In this example that is 1 kΩ || 10 kΩ || 10 kΩ = 833 Ω. For a 5.5 V supply and 0.4 V LOW, that means the buffer is sinking 16.3 mA."
I cannot see how 16.3mA was calculated. Using V=IR, to calculate current, I=V/R, 5V/833Ω = 6.1mA <- that's what I get.
Can someone help out here? Is this a typo or is my math off?
Please and thanks.